Unit Testing Support with VS Code?
Is there and/or will there be an approved off-target unit testing framework for STM32 (in my case, STM32H5)? I've been trying to stand up a test project generated by STM32CubeMX, imported into VS Code using Unity unit-testing framework, but running into pitfalls. In the past, I've used PlatformIO's with ease, was hoping the STM32 VSCode ext pack would be similar out the gate.
Over all, I'm aiming to test against the business logic and not needing a full-blown simulator. My rule of thumb is its good practice to do some kind of off-site (off-board) unit testing.
Even if there is a solid blog post with how to setup STM32 + CMake + Unity (or equivalent) and vanilla C using the CubeMX generated project, that would be most helpful. Most of the blog posts I find are either outdated, doing something custom, or a different architecture. Yes, I'll fully admit, my strong points are MSVC and C#'s tooling for test frameworks, and not so much with CMake/CTest.
Thank you!