Abnormal behaviour with STM32CubeMX
Hello,
Hope you're well. I started a project with CubeMX to use makefiles. I am able to compile and flash to the board but the code does not run properly on the f4 discovery board. To debug, I used Keil on a windows system and the code is actually working as expected(no changes made). Getting back to using make on my linux machine, the same code does not work properly on the board.
I then tried CubeIDE on linux and uploaded the code without any modifications and it works. So it leads me to believe that the problem is the cubemx generated makefile or it could be something else I am unaware about. I appreciate any help figuring this out, thank you.
Here is the current makefile
##########################################################################################################################
# File automatically-generated by tool: [projectgenerator] version: [4.5.0-RC5] date: [Mon Mar 10 15:10:23 EDT 2025]
##########################################################################################################################
# ------------------------------------------------
# Generic Makefile (based on gcc)
#
# ChangeLog :
# 2017-02-10 - Several enhancements + project update mode
# 2015-07-22 - first version
# ------------------------------------------------
######################################
# target
######################################
TARGET = f407
######################################
# building variables
######################################
# debug build?
DEBUG = 1
# optimization
OPT = -Og
#######################################
# paths
#######################################
# Build path
BUILD_DIR = build
######################################
# source
######################################
# C sources
C_SOURCES = \
Core/Src/main.c \
Core/Src/stm32f4xx_it.c \
Core/Src/stm32f4xx_hal_msp.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_tim.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_tim_ex.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_rcc.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_rcc_ex.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_flash.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_flash_ex.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_flash_ramfunc.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_gpio.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_dma_ex.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_dma.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_pwr.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_pwr_ex.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_cortex.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal.c \
Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_exti.c \
Core/Src/system_stm32f4xx.c \
Core/Src/sysmem.c \
Core/Src/syscalls.c
# ASM sources
ASM_SOURCES = \
startup_stm32f407xx.s
# ASM sources
ASMM_SOURCES =
#######################################
# binaries
#######################################
PREFIX = arm-none-eabi-
# The gcc compiler bin path can be either defined in make command via GCC_PATH variable (> make GCC_PATH=xxx)
# either it can be added to the PATH environment variable.
ifdef GCC_PATH
CC = $(GCC_PATH)/$(PREFIX)gcc
AS = $(GCC_PATH)/$(PREFIX)gcc -x assembler-with-cpp
CP = $(GCC_PATH)/$(PREFIX)objcopy
SZ = $(GCC_PATH)/$(PREFIX)size
else
CC = $(PREFIX)gcc
AS = $(PREFIX)gcc -x assembler-with-cpp
CP = $(PREFIX)objcopy
SZ = $(PREFIX)size
endif
HEX = $(CP) -O ihex
BIN = $(CP) -O binary -S
#######################################
# CFLAGS
#######################################
# cpu
CPU = -mcpu=cortex-m4
# fpu
FPU = -mfpu=fpv4-sp-d16
# float-abi
FLOAT-ABI = -mfloat-abi=hard
# mcu
MCU = $(CPU) -mthumb $(FPU) $(FLOAT-ABI)
# macros for gcc
# AS defines
AS_DEFS =
# C defines
C_DEFS = \
-DUSE_HAL_DRIVER \
-DSTM32F407xx
# AS includes
AS_INCLUDES =
# C includes
C_INCLUDES = \
-ICore/Inc \
-IDrivers/STM32F4xx_HAL_Driver/Inc \
-IDrivers/STM32F4xx_HAL_Driver/Inc/Legacy \
-IDrivers/CMSIS/Device/ST/STM32F4xx/Include \
-IDrivers/CMSIS/Include
# compile gcc flags
ASFLAGS = $(MCU) $(AS_DEFS) $(AS_INCLUDES) $(OPT) -Wall -fdata-sections -ffunction-sections
CFLAGS += $(MCU) $(C_DEFS) $(C_INCLUDES) $(OPT) -Wall -fdata-sections -ffunction-sections
ifeq ($(DEBUG), 1)
CFLAGS += -g -gdwarf-2
endif
# Generate dependency information
CFLAGS += -MMD -MP -MF"$(@:%.o=%.d)"
#######################################
# LDFLAGS
#######################################
# link script
LDSCRIPT = stm32f407vgtx_flash.ld
# libraries
LIBS = -lc -lm -lnosys
LIBDIR =
LDFLAGS = $(MCU) -specs=nano.specs -T$(LDSCRIPT) $(LIBDIR) $(LIBS) -Wl,-Map=$(BUILD_DIR)/$(TARGET).map,--cref -Wl,--gc-sections
# default action: build all
all: $(BUILD_DIR)/$(TARGET).elf $(BUILD_DIR)/$(TARGET).hex $(BUILD_DIR)/$(TARGET).bin
#######################################
# build the application
#######################################
# list of objects
OBJECTS = $(addprefix $(BUILD_DIR)/,$(notdir $(C_SOURCES:.c=.o)))
vpath %.c $(sort $(dir $(C_SOURCES)))
# list of ASM program objects
OBJECTS += $(addprefix $(BUILD_DIR)/,$(notdir $(ASM_SOURCES:.s=.o)))
vpath %.s $(sort $(dir $(ASM_SOURCES)))
OBJECTS += $(addprefix $(BUILD_DIR)/,$(notdir $(ASMM_SOURCES:.S=.o)))
vpath %.S $(sort $(dir $(ASMM_SOURCES)))
$(BUILD_DIR)/%.o: %.c Makefile | $(BUILD_DIR)
$(CC) -c $(CFLAGS) -Wa,-a,-ad,-alms=$(BUILD_DIR)/$(notdir $(<:.c=.lst)) $< -o $@
$(BUILD_DIR)/%.o: %.s Makefile | $(BUILD_DIR)
$(AS) -c $(CFLAGS) $< -o $@
$(BUILD_DIR)/%.o: %.S Makefile | $(BUILD_DIR)
$(AS) -c $(CFLAGS) $< -o $@
$(BUILD_DIR)/$(TARGET).elf: $(OBJECTS) Makefile
$(CC) $(OBJECTS) $(LDFLAGS) -o $@
$(SZ) $@
$(BUILD_DIR)/%.hex: $(BUILD_DIR)/%.elf | $(BUILD_DIR)
$(HEX) $< $@
$(BUILD_DIR)/%.bin: $(BUILD_DIR)/%.elf | $(BUILD_DIR)
$(BIN) $< $@
$(BUILD_DIR):
mkdir $@
#######################################
# clean up
#######################################
clean:
-rm -fR $(BUILD_DIR)
# Flash the STM32F4
burn: $(BUILD_DIR)/$(TARGET).bin
st-flash write $(BUILD_DIR)/$(TARGET).bin 0x8000000
#######################################
# dependencies
#######################################
-include $(wildcard $(BUILD_DIR)/*.d)
# *** EOF ***