About X-CUBE-IRREMOTE
Hi I am getting nowhere trying to use the X Cube IRRemote package, please help.
Should I expect the projects in en.x-cube-irremote\Projects\STM32G081B_EVAL to be imported into Cube IDE and run as a working example of the IR Remote functionality?
The readme file says:- "This example has been tested with STMicroelectronics STM32G081B-EVAL
boards and can be easily tailored to any other supported device
and development board."
Which makes me think it should just run.
If not can I please have some detailed description of how to make it work?
I have managed to get the point of one error in after building the project: unknown type name 'RC5_Frame_TypeDef' main.c Any instructions gratefully accepted.
When I read the readme file it says:
@par Directory contents
- TIM-Infrared/Src/main.c Main program
- TIM-Infrared/Src/menu.c Menu navigation implementation
- TIM-Infrared/Common_IR/Src/ir_common.c Functions shared for both IR protocols.
- TIM-Infrared/Common_IR/Src/rc5_decode.c RC5 receiver implementation
- TIM-Infrared/Common_IR/Src/sirc_decode.c SIRC receiver implementation
- TIM-Infrared/Common_IR/Src/rc5_encode.c RC5 transmitter implementation
- TIM-Infrared/Common_IR/Src/sirc_encode.c SIRC transmitter implementation
- TIM-Infrared/Src/system_stm32g0xx.c STM32G0xx system clock configuration file
- TIM-Infrared/Src/stm32g0xx_it.c Interrupt handlers
- TIM-Infrared/Src/stm32g0xx_hal_msp.c HAL MSP module
- TIM-Infrared/Inc/main.h Main program header file
- TIM-Infrared/Inc/menu.h Menu navigation header file
- TIM-Infrared/Inc/stm32g0xx_hal_conf.h HAL Configuration file
- TIM-Infrared/Inc/stm32g0xx_it.h Interrupt handlers header file
- TIM-Infrared/Common_IR/Inc/ir_common.h Shared definitions
- TIM-Infrared/Common_IR/Inc/rc5_decode.h RC5 receiver header file
- TIM-Infrared/Common_IR/Inc/sirc_decode.h SIRC receiver header file
- TIM-Infrared/Common_IR/Inc/rc5_encode.h RC5 transmitter header file
- TIM-Infrared/Common_IR/Inc/sirc_encode.h SIRC transmitter header file
I can't find that file structure.
Thanks in adavnce, Lance.