Bug in LL_ADC_SetAnalogWDThresholds()
Enabling analog watchdog 1 for ADC3 on a STM32H723 in CubeMX with low threshold 0x8 and high threshold 0x80 generates
LL_ADC_SetAnalogWDThresholds(ADC3, LL_ADC_AWD1, 0x80, 0x8);but the doc comment for LL_ADC_SetAnalogWDThresholds() says regarding the third parameter
* @param AWDThresholdsHighLow This parameter can be one of the following values:
* @arg @ref LL_ADC_AWD_THRESHOLD_HIGH
* @arg @ref LL_ADC_AWD_THRESHOLD_LOWindicating that the correct code to generate would be
LL_ADC_SetAnalogWDThresholds(ADC3, LL_ADC_AWD1, LL_ADC_AWD_THRESHOLD_HIGH, 0x80);
LL_ADC_SetAnalogWDThresholds(ADC3, LL_ADC_AWD1, LL_ADC_AWD_THRESHOLD_LOW, 0x8);However neither produces the desired result. The code generated by CubeMX sets the lower threshold to 8, whereas the code I assumed to be correct sets it to 0x88. The high threshold is left at the reset value of 0xFFF in both cases.
Looking at LL_ADC_SetAnalogWDThresholds() the line
MODIFY_REG(*preg,
AWDThresholdsHighLow,
AWDThresholdValue << ((AWDThresholdsHighLow & ADC_AWD_TRX_BIT_HIGH_MASK) >> ADC_AWD_TRX_BIT_HIGH_SHIFT4));seems to assume that AWDThresholdsHighLow is a bit mask, i.e. either 0x00000FFF for LL_ADC_AWD_THRESHOLD_LOW where the threshold should be stored in bits 11:0 or 0x0FFF0000 for LL_ADC_AWD_THRESHOLD_HIGH that should be stored in bits 27:16. The latter would then give
AWDThresholdsHighLow & ADC_AWD_TRX_BIT_HIGH_MASK ==
0x00000FFF & 0x00010000 = 0x00010000
and
(AWDThresholdsHighLow & ADC_AWD_TRX_BIT_HIGH_MASK) >> ADC_AWD_TRX_BIT_HIGH_SHIFT4) ==
0x00010000 >> 12 == 16
so that the threshold value is correctly shifted from 11:0 to 27:16.
The ADCx != ADC3 case seems to depend on AWDThresholdsHighLow being 0 or 1 though, so changing LL_ADC_AWD_THRESHOLD_HIGH/LOW to bit masks wouldn't work. But the MODIFY_REG() for ADC3 could maybe be changed to something like
uint32_t shift = AWDThresholdsHighLow << 4;
MODIFY_REG(*preg, 0xFFF << shift, AWDThresholdValue << shift);which seems to work.
Though to be honest, I'd rather have separate functions for high and low thresholds.
Using CubeMX version 6.7.0 and STM32Cube FW_H7 V1.11.0