Skip to main content
Sune Jensen
Associate II
December 13, 2023
Solved

[bug report] EXTI IRQ erroneously enabled when initializing in separate .h/.c files

  • December 13, 2023
  • 2 replies
  • 1727 views

STM32CubeMX version: 6.10.0

Firmware version: STM32Cube FW_G4 V1.5.1

 

I have configured a GPIO pin as EXTI and configured that the interrupt should not be enabled when initializing the GPIO, (i.e. removed the check mark from "Generate Enable in Init").

SuneJensen_2-1702456041392.png

If the initialization code is generated in main.c, the interrupt is not enabled (as expected).

// In main.c

static void MX_GPIO_Init(void)
{
 /* ... */

 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI0_IRQn, 5, 0);

 /* ... */
}

 

However, if the initialization code is generated in separate .h/.c files, the interrupt is erroneously generated.

SuneJensen_3-1702458375834.png

// In gpio.c

void MX_GPIO_Init(void)
{
 /* ... */

 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI0_IRQn, 5, 0);
 HAL_NVIC_EnableIRQ(EXTI0_IRQn);

 /* ... */
}
This topic has been closed for replies.
Best answer by Sune Jensen

Hey Mahmoud

I attached a minimum working example. It did yield some additional clues.

The problem only exists if more than a single pin is configured as EXTI.
If "Generate Enable in Init" is unchecked for all EXTI lines, the code is generated correctly. However, if at least a one line has the option checked, the IRQ is enabled for all lines.

My bug report seems to be a duplicate of https://community.st.com/t5/stm32cubemx-mcus/stm32cubemx-6-6-1-quot-generate-enable-in-init-quot-does-not/m-p/84845

I can however add the info that the bug only occurs if initialization code is generated in separate .h/.c files. When initialization is generated in main.c, only the desired IRQs are enabled.

2 replies

Technical Moderator
December 13, 2023

Hello @Sune Jensen ,

First let me thank you for posting.

I suggest that you provide your ioc.file for more investigation.

Thanks.

Mahmoud.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Sune Jensen
Sune JensenAuthorBest answer
Associate II
December 13, 2023

Hey Mahmoud

I attached a minimum working example. It did yield some additional clues.

The problem only exists if more than a single pin is configured as EXTI.
If "Generate Enable in Init" is unchecked for all EXTI lines, the code is generated correctly. However, if at least a one line has the option checked, the IRQ is enabled for all lines.

My bug report seems to be a duplicate of https://community.st.com/t5/stm32cubemx-mcus/stm32cubemx-6-6-1-quot-generate-enable-in-init-quot-does-not/m-p/84845

I can however add the info that the bug only occurs if initialization code is generated in separate .h/.c files. When initialization is generated in main.c, only the desired IRQs are enabled.

Technical Moderator
December 13, 2023

Hello,

I escalated the problem to CubeMx team in an internal ticket (ID: 168700 ) to take a closer look at this issue.

(PS: ID 168700 is an internal tracking number and is not accessible or usable by customers).

Thanks.

Mahmoud.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.