Build Error in STM32H747-DISCO Project with TouchGFX, CubeMX, and FreeRTOS
Hi all,
I encountered a build error while developing a TouchGFX project for the STM32H747-DISCO board. I followed these steps:
Steps to Reproduce:
Create a TouchGFX Project:
Used TouchGFX Environment on Windows to generate an empty STM32H747-DISCO project.
Added a background image and an Analog Clock.
Set the initial time of the clock to 00:00:00.
Clicked "Generate Code".
Modify the Project in STM32CubeMX:
Opened the project directory.
Used STM32CubeMX v6.14.0 to open the CubeMX project file.
Added the following peripherals:
CM4: RTC, OpenAMP, FreeRTOS
CM7: OpenAMP
Clicked "Generate Code" again.
Build in STM32CubeIDE:
Opened the project in STM32CubeIDE v1.18.0.
Attempted to build the CM7 project.
Encountered the following build error:
Build Error Output:
15:24:38 **** Incremental Build of configuration Debug for project STM32H747I-DISCO_CM7 ****
make all
arm-none-eabi-g++ -o "STM32H747I-DISCO_CM7.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"D:\TouchGFX_Project\STM32H7_RTC_Clock\STM32CubeIDE\CM7\STM32H747XIHX_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32H747I-DISCO_CM7.map" -Wl,--gc-sections -static -L../../../CM7/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group
...
D:/TouchGFX_Project/STM32H7_RTC_Clock/STM32CubeIDE/CM7/Debug/../../CM7/../../CM7/TouchGFX/generated/gui_generated/include/gui_generated/common/FrontendHeapBase.hpp:76:(.text._ZN16FrontendHeapBase15gotoStartScreenER19FrontendApplication[_ZN16FrontendHeapBase15gotoStartScreenER19FrontendApplication]+0x2): undefined reference to `FrontendApplicationBase::gotoScreen1ScreenNoTransition()'
...
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:101: STM32H747I-DISCO_CM7.elf] Error 1
"make all" terminated with exit code 2. Build might be incomplete.
15:24:38 Build Failed. 10 errors, 1 warnings. (took 532ms)Questions:
Why am I getting "undefined reference" errors related to TouchGFX components?
Could this be an issue with the integration of CubeMX and TouchGFX?
Is there a recommended workflow to correctly integrate FreeRTOS, OpenAMP, and RTC with TouchGFX?
Do I need to manually add missing TouchGFX files or update any settings in CubeIDE?
I would appreciate any suggestions or solutions to resolve this build issue. Thanks!