Configuring external SRAM for STM32H743 using CubeMX
Dear ST Community,
I need to use an SRAM with the STM32H743AII6 MCU. When I try to configure the project on CubeMX, a warning appears next to the FMC line. I feel like I should fix this before going further with the configuration.
I am curious why I am getting this warning even when FMC is the only peripheral that was already configured. Has anybody experienced this before? Are there any suggestions to resolve this?
Here is a summary as background information:
- The warning text says "Partly disabled conflict with FMC Chip Select NE1".
- Warning stays even if I use NE 2/3/4.
- The package is UFBGA169, and NE1 pin is available on that specific pinout.
- CubeMX version is 6.11.0 but the issue was present with earlier versions as well.
- A screenshot is attached below.
Thanks,
JD