Confused about MPU region config for STM32H5
I'm trying to set up a MPU region to block out DCACHE from my SDMMC1 peripheral but I notice whenever a region is activiated in CubeMX, the "region start" field will not let me type any hex value in. Some red text below says that region start must ALWAYS be 0x0. So my quesitons are:
1) If region start must always be 0x0, WHY is it a text field that I can enter something into?
2) Why must a region always start at 0x0? The region I want to block out from the DCACHE does not start at 0x0... I looked at some config documents for other chips (the example was an F7 i believe), and the MPU config allowed typing any hex value into the region start. I'm wondering if there's a bug here? Or maybe I just don't understand the H5 MPU enough.