Skip to main content
Associate
April 12, 2024
Solved

Cube MX having bug when setting up the ADC1 channels of STM32U575 in Diff Mode

  • April 12, 2024
  • 1 reply
  • 1161 views

Hi, 

 

This is my setup:

MCU: STM32U575OGY

STM32CubeIDE: 1.9.0

STM32CubeMX: 6.5.0-RC4

 

When setting up the ADC1 channels as Differential using the STM32CubeMX, it selects the GPIO pins that doesn't match with the GPIO mapping of the ADC1 in the datasheet. I manually set the channels and test the pins and datasheet is correct about the pins. So this seems like a bug in CubeMX. I am not sure if it has been fixed in updates or not.

Example: Setting up "ADC1- IN16 Differential" in CubeMX shows it is connected to "ADC1_IN15" and "ADC1_IN16". However; based on datasheet it is connected to ADC1_IN16 and ADC1_IN17. screenshots below. 

The problem with this issue is that CubeMX will lock up the wrong GPIO and won't let use it as another feature. In example below I cannot use the PB0 as anything else while it is not used. 

Sia1_0-1712936354290.png

Sia1_1-1712936368319.png

 

 

This topic has been closed for replies.
Best answer by AScha.3

Hi,

on

IDE 1.13.1

Cube 6.9.1

i just tried on U595 , seems ok:

AScha3_0-1712937393067.png

So do the update game ... and try then.

1 reply

AScha.3
AScha.3Best answer
Super User
April 12, 2024

Hi,

on

IDE 1.13.1

Cube 6.9.1

i just tried on U595 , seems ok:

AScha3_0-1712937393067.png

So do the update game ... and try then.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Sia1Author
Associate
April 12, 2024

Yes; I tried the update Cube MX and I didn't the issue there.