CubeIDE 1.16.0 (MX6.12.0) STM32G0B1CCU ADC1 poblem
Hi,
I have tried to load a Project (.ioc file) build with CubeIDE 1.15.0 in the newly released CubeIDE1.16.0 (with CubeMX 6.12.0).
This give me an error on ADC1:
1) I can't select Vbat as ADC source (as working on CubeMX 6.11.0)
2) I get a warning about ADC_Regulare_ConversationMode
The attached picture shows to the left the 1.16.0 and to right the 1.15.0 version

Is this a known problem with the CubeMX 6.12.0?