Question
CubeMX 6.13.0 and MCU Package H7 v1.12.0 produce incorrect PCLK frequencies
I updated to CubeMX 6.13.0 and firmware package 1.12.0 for and STM32H755BIT chip and found several issues with the new release:
- Where is it documented that the new ExitRun0Mode() requires 'USE_PWR_LDO_SUPPLY" to be defined if I want to use that mode? Shouldn't it be defined by CubeMX when the power parameters are selected in the RCC section?
- If I am using the Voltage regulator in the LDO supply mode (see RM0399, p 274, Fig. 22, Section 1), what is the purpose of defining SMPS in line 217 of stm32h755xx.h? In line 440 of system_stm32h7xx_dualcore_boot_cm4_cm7.c the define of SMPS is used to disable the SMPS - shouldn't the define be used to enable the SMPS?
- Worst issue: The clock rates returned from PCLK function calls shown below are now showing 240 MHz! This has messed up the USARTs and all the timers. I thought the MAX clock rate for the PCLK clocks were 120 MHz (see DS12919, p. 110, Table 23, fPCLK, at VOS0 setting).
HAL_RCC_GetPCLK1Freq();
HAL_RCC_GetPCLK2Freq();
Screen capture showing 240 MHz clock rate on PCLK: