Skip to main content
Associate II
April 4, 2025
Solved

CubeMX 6.14 generate OpenAMP error in STM32H747 error.

  • April 4, 2025
  • 7 replies
  • 1121 views

Hi all,

I am using CubeMX 6.14 to generate an OpenAMP project for the STM32H747I-DISCO board. When I build the project, I receive the following warnings, and it results in an 'OpenAMP create endpoint' error at runtime. I used the same code and project created with CubeMX 6.12, and it works fine. Therefore, I suspect there might be an issue with CubeMX 6.14. Could someone please advise me on how to generate a working OpenAMP project using CubeMX?

arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc.o"
<command-line>: warning: "RPMSG_BUFFER_SIZE" redefined
<command-line>: note: this is the location of the previous definition
arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc_ex.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc_ex.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc_ex.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc_ex.o"
<command-line>: warning: "RPMSG_BUFFER_SIZE" redefined
<command-line>: note: this is the location of the previous definition
arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rtc.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc.o"
<command-line>: warning: "RPMSG_BUFFER_SIZE" redefined
<command-line>: note: this is the location of the previous definition
arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rtc_ex.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc_ex.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc_ex.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc_ex.o"
<command-line>: warning: "RPMSG_BUFFER_SIZE" redefined
<command-line>: note: this is the location of the previous definition
arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim.o"
<command-line>: warning: "RPMSG_BUFFER_SIZE" redefined
<command-line>: note: this is the location of the previous definition
arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim_ex.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim_ex.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim_ex.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim_ex.o"
<command-line>: warning: "RPMSG_BUFFER_SIZE" redefined
Best answer by sirhc79

So there is a wrong (re)definition of RPMSG_BUFFER_SIZE in the project settings. A temporary solution is to remove it from the project settings for both cores and recompile. 

sirhc79_0-1745230283786.png

Regards, 

Chris

 

7 replies

Ghofrane GSOURI
Technical Moderator
April 4, 2025

Hello @Tom17 

First let me thank you for posting.

I'm currently checking this issue internally,  I will get back to you asap.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
April 8, 2025

Hi Ghofrane,

I also encountered the same problem, is there a solution to this problem?

Ghofrane GSOURI
Technical Moderator
April 9, 2025

Hello @Tom17 

Issue has been raised to dev team .

Internal ticket number : 207197

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tom17Author
Associate II
April 9, 2025

Hi @Ghofrane GSOURI ,

Since my project is quite urgent, I was wondering if you could provide a workaround or a method for manual modification?

NickO
Associate III
April 9, 2025

Same for Cube IDE v1.18

Tom17Author
Associate II
April 15, 2025

This bug is still present in version 6.14.1 and hasn't been resolved. Is there a plan to fix it?

sirhc79Best answer
Visitor II
April 21, 2025

So there is a wrong (re)definition of RPMSG_BUFFER_SIZE in the project settings. A temporary solution is to remove it from the project settings for both cores and recompile. 

sirhc79_0-1745230283786.png

Regards, 

Chris

 

Tom17Author
Associate II
April 21, 2025

Hi Chris,

Thank you for your explanation. The issue has been resolved.