CubeMX 6.16.0 generates conflicting CMake configuration
The CubeMX 6.16.0 is able to generate a CMake-project for an STM32H7 - great. A small conflict currently exists in the following two generated files [for a "basic" STM32H7 project]:
- CM7/CMakeLists.txt:69
# Add linked libraries
target_link_libraries(${CMAKE_PROJECT_NAME} PRIVATE
# Add user defined libraries
)- CM7/mx-generated.cmake:81
# Add libraries to the project
target_link_libraries(${CMAKE_PROJECT_NAME} ${MX_LINK_LIBS})
The first specifies
PRIVATEwhile the second does not - which is incompatible as per CMake.
Can someone confirm this observation?
Can this be made consistent in the future? If so, I would prefer the one with the scope keyword - but could also live without it here.