Question
CubeMX and STM32H753I-EVAL2 issues
Having some issues with CubeMX not showing properly the DevKit hardware features. For example:
- The devkit has an ST-LINK V3 chip (per documentation and according to silk screen) yet CubeMX has the ST-LINK V2 setting available only, ST-LINK V3 is greyed out ?!?
- The crypto engine per documentation supports e.g. HMAC, yet it is greyed out in CubeMX
- External Flash shows as 1152 Mbit in CubeMX which is incorrect, yet it is fixed/unchangeable.
- Don't see the SDRAM (8Mx32bit) and SRAM (1M x 16bit) as a separate item in CubeMX
Both the STM32CubeMX and the H7 package has the latest version on my computer 6.21.1 & 1.11.2 respectively.
Running under Win11 Pro.
Any help is appreciated.
Thanks