Skip to main content
MSilv
Visitor II
June 10, 2024
Question

CUBEMX bug with auto-generated include in main.h for Nucleo H563 missing carriage return

  • June 10, 2024
  • 1 reply
  • 931 views

Hi, I'm using the latest build of CUBEMX 6.11.1 using firmware package STM32Cube FW_H5 V1.2.0 along with Keil MDK uVision V5.39.0.0.  My target micro is the STM32H563ZIT6 (Nucleo H563).  I've encountered a repeatable problem with this build of CUBEMX where it does not properly include a carriage return at the end of the include for the "stm32h5xx_nucleo.h" header file.  Of course, if I don't first fix this error before I try to compile, numerous errors are generated and the compile fails.

Here's the problem in my main.h with the automatically generated include statements:

/* Includes ------------------------------------------------------------------*/
#include "stm32h5xx_hal.h"
#include "stm32h5xx_nucleo.h"#include "stm32h5xx_ll_dma.h"
#include "stm32h5xx_ll_crs.h"
#include "stm32h5xx_ll_rcc.h"
#include "stm32h5xx_ll_bus.h"
#include "stm32h5xx_ll_system.h"
#include "stm32h5xx_ll_exti.h"
#include "stm32h5xx_ll_cortex.h"
#include "stm32h5xx_ll_utils.h"
#include "stm32h5xx_ll_pwr.h"
#include "stm32h5xx_ll_spi.h"
#include "stm32h5xx_ll_tim.h"
#include "stm32h5xx_ll_usart.h"
#include "stm32h5xx_ll_gpio.h"

(end of code snippet)

Once I've moved the errantly located #include to its own line, the project compiles normally.

Thank you,

1 reply

Technical Moderator
June 11, 2024

Hello @MSilv ,

First let me thank you for posting and welcome to the ST Community.

For more investigation, I suggest that you provide the ioc.File.

Thanks.

Mahmoud.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.