CubeMX doesn't generate .project and .cproject files with non-default firmware location
CubeMX does not generate .project and .cproject files for cubeIDE, when in CubeMX project it is selected to not use default firmware location, and path set to folder with STM32Cube FW from github.
To reproduce:
1 Open CubeMX
2 Select File->New Project
3 Select chip, in my case stm32g491ceu6
4 Open Project manager tab, enter name and location for the project, toolchain - stcubeide
5 Uncheck "Use Default Firmware Location", Click Browse and navigate to a folder with github repository with cude FW package
6 Go to "Code Generator" sub tab, select radio button "Add nevessary library files as reference in the toolchainproject configuration file"
7 Click generate
8 Observe folder content in the file explorer - .cproject and .project are missing.
CubeMX version 6.16.1