CubeMX I2C stupid UX issue
Every time I need to configure I2C, which is not often, I have to check the correct rise and fall times for the default 100kHz frequency and doing so I am asking myself a question why the typical 100kHz value is provided by default but rise and fall times are not, when most of the time 1000 and 300ns values are needed and I2C will NOT work with default values 0. Would not it increase user experience if the correct, typical values were provided in addition to the typical clock frequency?
Btw, CubeMX calculated timings are slightly off the I2C specs and conditions defined in ST RM docs. I believe the CubeMX algorithm is incorrect. Therefore I suggest to always enable the 'advanced settings' and allow the user to enter timings manually. Explaining why the calculation algorithm is incorrect is beyond the scope of this post.