CubeMx V6.6.1 - Windows 11: Issues with toolchain location folder and Makefile toolchain
Hi,
In CubeMx V6.6.1 - Windows 11 i am having the 2 following issues.
- In Project Management if i select Makefile as the Toolchain / IDE then i cannot access the toolchain location folder to make it a new location, the input box is not enabled.
- To work around the point above i do the following steps:
- choose first EWARM as Toolchain / IDE
- update the Toolchain location folder
- choose Makefile as Toolchain / IDE
- Generate the code
Until this point all goes ok and the toolchain files are correctly generated in the toolchain folder.
But if i close CubeMx project and reopen it again the toolchain location is lost.
I looked inside the project.ioc file and it is correctly stored there.
It seems like this might be a bug.
Thanks
Paulo