Custom packs path in IOC files
I've been using CubeMX for the last 2.5 years and am in the process of updating our ioc files to the latest version of the CubeMX software, the latest STM32 Firmware and to use AzureRTOS rather than the old ThreadX and NetX releases from Express Logic.
Whilst I am familiar with being able to set a custom path for the STM32 Firmware in Project Manager -> Project -> Mcu and Firmware Package -> Fimware Relative Path to: C:\ThirdPartyCode\STM32Cube\Repository\STM32Cube_FW_F4_V1.28.0 for example I cannot work out how to set a custom location for other packages such as AzureRTOS.
As such the IAR project files that are generated then contain include paths to X-CUBE-AZRTOS-F4 under the local user directory. For example:
C:/Users/Developer/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AZRTOS-F4/1.1.0/Middlewares/ST/netxduo/common/drivers/ethernet/
C:/Users/Developer/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AZRTOS-F4/1.1.0/Middlewares/ST/netxduo/common/inc/
C:/Users/Developer/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AZRTOS-F4/1.1.0/Middlewares/ST/netxduo/ports/cortex_m4/iar/inc/
C:/Users/Developer/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AZRTOS-F4/1.1.0/Middlewares/ST/threadx/common/inc/
C:/Users/Developer/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AZRTOS-F4/1.1.0/Middlewares/ST/threadx/ports/cortex_m4/iar/inc/
There also seems to be a couple of minor bugs in the path generation (although they don't affect functionality)
a) There is a double slash between the 'Repository' directory and the 'Packs' sub-directory.
b) There is a trailing slash at the end of the path, that is unnecessary (and doesn't exist for the generated STM32 Firmware Path.