Skip to main content
therealergo
Associate II
March 2, 2026
Solved

DMA Setup not Generated on STM32N6

  • March 2, 2026
  • 1 reply
  • 149 views

With HPDMA configured for SAI1A, no DMA setup code is generated with CubeMX 6.17.0. See attached IOC file as an example. Possible that I'm missing a required setting, but I can't find anything.

Edit: Fully deleting and re-creating project seems to have fixed it :shrug:.

Best answer by Ghofrane GSOURI

Hello @therealergo 

Thank you for your contribution.

Sometimes the IOC file can become corrupted. Since you fully deleted and re-created the project and everything then worked as expected, this behavior does not appear to be a CubeMX bug in this case.

THX

Ghofrane

 

1 reply

Ghofrane GSOURI
Ghofrane GSOURIBest answer
Technical Moderator
March 3, 2026

Hello @therealergo 

Thank you for your contribution.

Sometimes the IOC file can become corrupted. Since you fully deleted and re-created the project and everything then worked as expected, this behavior does not appear to be a CubeMX bug in this case.

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.