Skip to main content
Andrei Chichak
Lead
May 2, 2025
Question

F469 SD initialization bug with F4 FW 1.28.1

  • May 2, 2025
  • 1 reply
  • 537 views

I'm putting together a small test program in CubeIDE 1.18.1, CubeMX 6.14.1, on Intel MacOS 15.4.1 on a STM32F469I-DISCO and I've noticed some (possibly) incorrect SDIO initialization code.

Cube generated this:

void MX_SDIO_SD_Init(void)
{

 /* USER CODE BEGIN SDIO_Init 0 */

 /* USER CODE END SDIO_Init 0 */

 /* USER CODE BEGIN SDIO_Init 1 */

 /* USER CODE END SDIO_Init 1 */
 hsd.Instance = SDIO;
 hsd.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
 hsd.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
 hsd.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
 hsd.Init.BusWide = SDIO_BUS_WIDE_4B;
 hsd.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
 hsd.Init.ClockDiv = 0;
 if (HAL_SD_Init(&hsd) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_SD_ConfigWideBusOperation(&hsd, SDIO_BUS_WIDE_4B) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SDIO_Init 2 */

 /* USER CODE END SDIO_Init 2 */

}

and it always calls Error_Handler at line 24 with an error value of 0x0400'0000 (SDMMC_ERROR_REQUEST_NOT_APPLICABLE).

Notice that the HAL_SD_Init call on line 18 uses the .BusWide value of SDIO_BUS_WIDE_4B on line 15. Notice that on line 22 it calls to set up the bus for the same 4B width. It doesn't like that. I suspect that the bus is already set up for 4-bit width and doesn't like being told to set it up for 4-bit width.

If you look in the demo program that works, Fx_uSD_File_Edit, you can see that they initially use SDIO_BUS_WIDE_1B for the Init, then switch to 4B. If I change my code to use 1B, it succeeds and the card can be opened successfully.

A regression at some point?

Thanks,

Andrei (Your neighbour from The Great White North)

1 reply

KDJEM.1
Technical Moderator
May 8, 2025

Hello @Andrei Chichak ;

 

This issue is already reported internally.

Internal ticket number: 155983 (This is an internal tracking number and is not accessible or usable by customers)

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.