FreeRTOS SysTick_Handler missing
Moved from MPUs forum; STM32F072 is an MCU - not an MPU.
Hi,
I've just started a new project for a STM32F072 chip using STM32CubeIDE 1.17.0.
When adding FreeRTOS support to my project, the program hangs soon after osKernelStart() is called.
I had hard time finding the culprit.
The problem is that the SysTick_Handler() present in cmsis_os2.c is not used (It is surrounded with #if defined(SysTick) / #endif).
Because os this, the default handler is called (infinite while loop).
I've worked around this problem by copying the SysTick_Handler() function in my code. But this problem should be fixed in the STM32CubeIDE code generator.
Best regards,
Nicolas