how to configure fileX with threadX
Hi, all
I am using NUCLEO-U575ZI-Q.
I have the same problem with this post.
https://community.st.com/t5/stm32cubemx-mcus/how-to-configure-filex-using-cubemx/m-p/590201#M25964
Now, I upgraded my CubeMx from 6.10.0 to 6.11.1, CubeIDE's version is 1.14.0.
I still have problem to open the media.
Do you have a sample code of FileX and threadX to test?
ps: I am sure it is not hardware issue, as it can run Fx_File_Edit_Standalone (only FileX, no threadX) to create file sucessfully.
Thanks in advance.
Victor