Adding compile definitions, adding include paths and removing source files
The generated CMakeLists.txt files are cmake interface libraries and not compiled libraries. They are basically a list of source files and compile definitions. When they are included in your ./CMakeLists.txt this information can be modified without modifying those files. This is what you want, because you don't want to constantly have to manually change (re)generated files.
Add the following sections to your ./CMakeLists.txt file:
# modifications to stm32cubemx interface library without modifying its CMakeLists.txt file:
# add a define to stm32cubemx interface libary:
target_compile_definitions(stm32cubemx INTERFACE
<additional definitions for stm32cubemx>
)
# Add extra include directories to stm32cubemx interface library:
target_include_directories(stm32cubemx INTERFACE
<additional includes for stm32cubemx>
)
# Remove sources from stm32cubemx interface library:
get_target_property(APP_SOURCES ${CMAKE_PROJECT_NAME} SOURCES)
list(REMOVE_ITEM APP_SOURCES
<sources to remove from stm32cubemx>
)
set_property(TARGET ${CMAKE_PROJECT_NAME} PROPERTY SOURCES "${APP_SOURCES}")
# Remove sources from STM32_Drivers:
get_target_property(APP_SOURCES STM32_Drivers SOURCES)
list(REMOVE_ITEM APP_SOURCES
<sources to remove from STM32_Drivers used by stm32cubemx>
)
set_property(TARGET STM32_Drivers PROPERTY SOURCES "${APP_SOURCES}")
# Remove sources from USB_Host_Library:
get_target_property(APP_SOURCES USB_Host_Library SOURCES)
list(REMOVE_ITEM APP_SOURCES
<sources to remove from USB_Host_Library used by stm32cubemx>
)
set_property(TARGET USB_Host_Library PROPERTY SOURCES "${APP_SOURCES}")
Example:
# modifications to stm32cubemx interface library without modifying its CMakeLists.txt file:
# add a define to stm32cubemx interface library:
target_compile_definitions(stm32cubemx INTERFACE
HTTPD_FSDATA_FILE="../httpd/fsdata.c"
)
# Add extra include directories to stm32cubemx interface library:
target_include_directories(stm32cubemx INTERFACE
httpd
Communication
Config
Common
Process
Display
)
# Remove sources from stm32cubemx interface library:
get_target_property(APP_SOURCES ${CMAKE_PROJECT_NAME} SOURCES)
# message(WARNING ${APP_SOURCES}) # optional print statement before
list(REMOVE_ITEM APP_SOURCES
${CMAKE_CURRENT_SOURCE_DIR}/cmake/stm32cubemx/../../USB_HOST/App/usb_host.c
${CMAKE_CURRENT_SOURCE_DIR}/cmake/stm32cubemx/../../TouchGFX/target/generated/OSWrappers.cpp
)
# message(WARNING ${APP_SOURCES}) # optional print statement after
set_property(TARGET ${CMAKE_PROJECT_NAME} PROPERTY SOURCES "${APP_SOURCES}")
# Remove sources from STM32_Drivers:
get_target_property(APP_SOURCES STM32_Drivers SOURCES)
# message(WARNING ${APP_SOURCES}) # optional print statement before
list(REMOVE_ITEM APP_SOURCES
${CMAKE_CURRENT_SOURCE_DIR}/cmake/stm32cubemx/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_hcd.c
${CMAKE_CURRENT_SOURCE_DIR}/cmake/stm32cubemx/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_ll_usb.c
)
# message(WARNING ${APP_SOURCES}) # optional print statement after
set_property(TARGET STM32_Drivers PROPERTY SOURCES "${APP_SOURCES}")
# Remove sources from USB_Host_Library:
get_target_property(APP_SOURCES USB_Host_Library SOURCES)
# message(WARNING ${APP_SOURCES}) # optional print statement before
list(REMOVE_ITEM APP_SOURCES
${CMAKE_CURRENT_SOURCE_DIR}/cmake/stm32cubemx/../../Middlewares/ST/STM32_USB_Host_Library/Core/Src/usbh_core.c
${CMAKE_CURRENT_SOURCE_DIR}/cmake/stm32cubemx/../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Src/usbh_msc.c
)
# message(WARNING ${APP_SOURCES}) # optional print statement after
set_property(TARGET USB_Host_Library PROPERTY SOURCES "${APP_SOURCES}")
Output a graph with library dependencies
You can generate a dependency graph of your CMake project:
# add_custom_command(TARGET ${CMAKE_PROJECT_NAME} POST_BUILD
COMMAND ${CMAKE_COMMAND} "--graphviz=cmake_dependency_graph.dot" .
COMMAND dot -Tpng cmake_dependency_graph.dot -o cmake_dependency_graph.png
WORKING_DIRECTORY "${CMAKE_BINARY_DIR}"
)This graph will contain all the library and executable dependencies in the project showing the dependencies between the targets in a project, as well as external libraries which are linked against.
This will generate something like:

With me it works, but it requires a successful build first. There is some type of racing condition. So I need to comment it out first, build and then I can uncomment it again. If you know how to do this let me know.
Remove external FLASH sector from elf file to speed up debugging sessions
My TouchGFX project uses external flash. In order to debug without always flashing the entire external flash you can create a separate elf file that has those sections removed. You can use the following command for that:
add_custom_command(TARGET ${CMAKE_PROJECT_NAME} POST_BUILD
COMMAND ${CMAKE_OBJCOPY} ${CMAKE_PROJECT_NAME}.elf ${CMAKE_PROJECT_NAME}_NO_OFLASH.elf --remove-section=.textoctoflash --remove-section=ExtFlashSection
WORKING_DIRECTORY "${CMAKE_BINARY_DIR}"
)This saves a lot of time when debugging.