Skip to main content
porter.chen
Associate
August 4, 2022
Question

How to make the right connection for using DDR Test Suite?

  • August 4, 2022
  • 14 replies
  • 5013 views

0693W00000QMwtvQAD.jpg0693W00000QMx0DQAT.jpgThe board is installed with the system( stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15) by following the Getting started .

0693W00000QMx03QAD.jpgAll drivers are installed.

However, in the DDR test suite, I cannot connect to the device.

How to make the right connection for using DDR Test Suite?

Do I need a DDR utilities binary file for the connection?

thank you

This topic has been closed for replies.

14 replies

Erwan SZYMANSKI
Technical Moderator
August 9, 2022

Hello @porter.chen​ ,

Can you double check if you well followed all the steps explained at this link ? There are some paragraphs that deals with your issue.

Regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Semer CHERNI
ST Employee
August 9, 2022

Hello @porter.chen​ 

First le me thank you for having reported.

The link posted by @Erwan SZYMANSKI​  is very helpful.

I just want to add the steps I have done in details:

  1. Put the SW1 to [1 0 1 0] 
  2. Flash the MP135 with the "STM32MP135C-DK_DDR_UTILITIES_A7_signed.stm32" file found under this https://github.com/STMicroelectronics/STM32DDRFW-UTIL/tree/main/Binaries/STM32MP135C-DK_DDR_UTILITIES_A7 with the Cube programmer in CLI using this cmd "Cubeprogrammer install path\STM32_Programmer_CLI.exe -c port=usb1 -w the file path\STM32MP157C-DK2_DDR_UTILITIES_A7_signed.stm32 0x01 --start 0x01"
  3. In the CubeMX under [Tools] [DDR Test Suite] check SYSRAM Loading and add "STM32MP135C-DK_DDR_UTILITIES_A7_signed.stm32" to [DDR utilities binary file]
  4. Click on connect and it should work fine

Regards,

Semer.

porter.chen
Associate
August 11, 2022

@Erwan SZYMANSKI​ @Semer CHERNI​ 

Thank you for the support.

  • I modified SW1  [0 0 0 0] and followed the steps from 1 to 2. Then followed step 3 and 4 with SW1[1010], but it shows errors in activating device and no responding

  • Will it cause the connection problem when applying STM32MP135C-DK_DDR_UTILITIES_A7_signed.stm32 to the board STM32MP135F-DK?

Could you help?0693W00000QNTz3QAH.jpg0693W00000QNTx4QAH.jpg0693W00000QNTzrQAH.jpgThank you

porter.chen
Associate
August 12, 2022

@Erwan SZYMANSKI (ST Employee)​ @Semer CHERNI (ST Employee)​ 

Thank you for the support.

 0693W00000QNTyeQAH.jpg0693W00000QNXf7QAH.jpg0693W00000QNXfHQAX.jpgThen changed SW1 to [0010], [1010] and reboot, try to connect, but the same, it shows "This Port Com Is Not Responding".

  • After that, I used SW1[1 0 1 0] by following "3.2.5.1.2 Serial boot"., but it shows "This Port Com Is Not Responding" and "Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again…"

Then I tried SW1 [0 0 1 0] and repeat  "3.2.5.1.2 Serial boot"; and tried SW1[0 0 0 0] and repeat  "3.2.5.1.2 Serial boot". It shows the same "This Port Com Is Not Responding" and "Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again…"

 0693W00000QNXfMQAX.jpg 

  • The com port information is shown in the attached picture. How to check the​ serial port is properly connected?

0693W00000QNXfRQAX.jpg 

  • Will it cause the connection problem when applying STM32MP135C-DK_DDR_UTILITIES_A7_signed.stm32 to the board STM32MP135F-DK?

0693W00000QNXfWQAX.jpg

​Could you help?

Thank you

porter.chen
Associate
August 12, 2022

Adding the information I got from SW1 operating instruction

Force USB boot for flashing SW1[0 0 0 0]

Engineering boot SW1[0 0 1 0]

Boot from microSD card SW1[1 0 1 0]

0693W00000QNXgtQAH.jpg 

porter.chen
Associate
August 19, 2022

Hi @Erwan SZYMANSKI (ST Employee)​ @Semer CHERNI (ST Employee)​ 

Could you help check if any process is missing to make a proper connection?

Thank you

Semer CHERNI
ST Employee
August 26, 2022

Hello @porter.chen​ 

First sorry because my response took time.

About how to connect the board and run the DDR test Suite I found a roughly simple way:

  1. Start by downloading this repo GitHub - STMicroelectronics/STM32DDRFW-UTIL: DDRFW-UTIL tool repository
  2. Put the board in engineering mode 0693W00000Sts8QQAR.png
  3. Using STM32CubeIDE import the project "STM32MP135C-DK" I used this project on STM32MP135F because I couldn't find an other one(you can follow the steps described in 2.2 How to compile and launch DDR Tool project)
  4. Build the imported project and run it
  5. Open CubeMX and follow the steps described in 2.2 How to compile and launch DDR Tool project

Kind regards,

Semer.

porter.chen
Associate
September 13, 2022

Hi @Semer CHERNI​ ,

Thank you for the information.

It does not work properly, details of the operation are listed below.

Could you help?

2.2.2 Build project

The project can contain several build configurations. In that case, you should firstly select the configuration corresponding to your hardware version:

  • Right click on the project in the Project Explorer
  • Go to Build configurations > Set Active
  • Select your configuration0693W00000SvEPLQA3.jpg

To build the project in STM32CubeIDE:

  • Right click on the project in the Project Explorer
  • And click on "Build Project"

0693W00000SvEPfQAN.jpg2.2.3 Launch project

To launch the project:

  • Right click on the project in the Project Explorer
  • Select "Debug As / Debug Configurations�?
  • 0693W00000SvEQ9QAN.jpg
  • In STM32 Cortex-M C/C++ Application / Select your debug configuration (if not present, double-click on "STM32 Cortex-M C/C++ Application")
  • In Main tab:
    • Make sure binary file .elf is correctly set
    • 0693W00000SvEaiQAF.jpg
  • In Debugger tab:
    • Make sure JTAG/SWD link (Engineering mode) is selected for "Load Mode"
    • Debug probe uses ST-LINK
    • 0693W00000SvEasQAF.jpg
    • 0693W00000SvEbHQAV.jpg
  • On your board, make sure the boot pins are set in Engineering mode (See §2.1 Hardware connections)
  • Then launch the Debug session
  • 0693W00000SvEbvQAF.jpg

​ failure information:

Open On-Chip Debugger 0.11.0+dev-00449-g53fa0f7 (2022-06-09-09:42) [https://github.com/STMicroelectronics/OpenOCD]

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V3J8M3B5S1 (API v3) VID:PID 0483:3753

Info : Target voltage: 3.310621

Info : Unable to match requested speed 5000 kHz, using 3300 kHz

Info : Unable to match requested speed 5000 kHz, using 3300 kHz

Info : clock speed 3300 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : STM32MP135FAFx.cpu: hardware has 6 breakpoints, 4 watchpoints

Info : STM32MP135FAFx.cpu: MPIDR level2 0, cluster 0, core 0, multi core, no SMT

Info : gdb port disabled

Info : gdb port disabled

Info : starting gdb server for STM32MP135FAFx.cpu on 3333

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

Info : New GDB Connection: 1, Target STM32MP135FAFx.cpu, state: halted

Info : rejected 'gdb' connection, no more connections allowed

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : stlink_dap_op_connect(connect)

Info : stlink_dap_op_connect(reconnect)

Info : SWD DPIDR 0x6ba02477

target halted in ARM state due to debug-request, current mode: Supervisor

cpsr: 0x200001d3 pc: 0x0000a97c

MMU: disabled, D-Cache: disabled, I-Cache: disabled

3.Build the imported project and run it

0693W00000SvEeLQAV.jpg0693W00000SvEfnQAF.jpg failure information:

Open On-Chip Debugger 0.11.0+dev-00449-g53fa0f7 (2022-06-09-09:42) [https://github.com/STMicroelectronics/OpenOCD]

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V3J8M3B5S1 (API v3) VID:PID 0483:3753

Info : Target voltage: 3.313828

Info : Unable to match requested speed 5000 kHz, using 3300 kHz

Info : Unable to match requested speed 5000 kHz, using 3300 kHz

Info : clock speed 3300 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : STM32MP135FAFx.cpu: hardware has 6 breakpoints, 4 watchpoints

Info : STM32MP135FAFx.cpu: MPIDR level2 0, cluster 0, core 0, multi core, no SMT

Info : gdb port disabled

Info : gdb port disabled

Info : starting gdb server for STM32MP135FAFx.cpu on 3333

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

Info : New GDB Connection: 1, Target STM32MP135FAFx.cpu, state: halted

Info : rejected 'gdb' connection, no more connections allowed

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : stlink_dap_op_connect(connect)

Info : stlink_dap_op_connect(reconnect)

Info : SWD DPIDR 0x6ba02477

target halted in Thumb state due to debug-request, current mode: Supervisor

cpsr: 0x200001f3 pc: 0x000060a4

MMU: disabled, D-Cache: disabled, I-Cache: disabled

shutdown command invoked

4.Open CubeMX and follow the steps described in 2.2 How to compile and launch DDR Tool project

=> The port com is not responding

​Thank you

Semer CHERNI
ST Employee
September 13, 2022

Hello @porter.chen​ 

Thanks for your feedback.

I think that there are 2 main reasons for the failure:

  • The project structure in the screenshots you posted is a little different that the one I have:

0693W00000SvFKqQAN.png 

==> Make sure you imported the project this way :

  • Go to File > Import
    • Select "Existing Projects into Workspace" > Next
    • Browse to your project location (In the STM32DDRFW-UTIL package, the projects are stored in DDR_Tool directory)
    • Select one of the listed project > Finish

  • When debugging I see that you get an error about a failure in activating the live expressions

==> When the "Enable live expressions" is selected I get the same error message when debugging

==> Make sure that this option is disabled in the debug configuration

0693W00000SvFMcQAN.png 

Kind regards,

Semer.

porter.chen
Associate
September 14, 2022

Hi @Semer CHERNI​ 

Thank you for the information.

The the listed projects are gray and cannot be selected. "Finish" can not be selected. Could you help?

  • Go to File > Import
    • Select "Existing Projects into Workspace" > Next
      • 0693W00000SvJStQAN.jpg
    • Browse to your project location (In the STM32DDRFW-UTIL package, the projects are stored in DDR_Tool directory)
      • 0693W00000SvJTDQA3.jpg
    • Select one of the listed project > Finish
      • the listed projects are gray and cannot be selected
      • => cannot "finish"

0693W00000SvJThQAN.jpg 

​Thank you

Alex - APMemory
Associate II
November 9, 2022

Hi @Semer CHERNI (ST Employee)​

Any chance to help on this issue?

Thanks