How to Set VREFBUF to Internal Voltage Refence
I'm using at STM32H563VITz in LQFP100 package.
According to the reference manual (RM0481 Rev 21209) I can use the internal Voltage Reference (and then set it to 2.0478V)


I've also referenced the post at: How to configure VREFBUF on my STM32 - STMicroelectronics Community
When I open the .ioc file for my project. I don't have the option to select the Internal Voltage Reference

It could be a bug in Cube MX - but I suspect it's more likely that I haven't enabled some component or peripharl in the .ico file?