Question
In RM0401 Rev 3 and using the STM32F410, Table 62 page 373 shows that LPTIM can be used as a source trigger for TIM5 (slave). Is this possible?
I've noticed that there does not seem to be a trigger output selection for LPTIM. Is there a default operation I am missing?
I've tried making LPTIM as the source trigger for TIM5 for the STM32F410 in the CubeMX IDE but can't seem to get it to work.
If this is possible, is there an example setup I can refer too?