Invalid SRAM6 Warning for U5A5ZJT6Q
Operating System: Windows 10
STM32CubeMX version: 6.10.0
STM32CubeU5 Firmware Package V1.4.0 / 20-October-2023
When I attempt to validate my X-CUBE-AI model on target, I receive the following pop-up:

Exploring STM32CubeMX.log shows the following warning:
[WARN] IP:2119 - SRAM6PowerDownInRunMode not found: check if there is a RefParameter without a condition.
The U5A5 doesn't even have an SRAM6, if I am reading the datasheet correctly. When I look at the configuration options in CubeMX, I can't see anything for SRAM6 in the PWR section.