Skip to main content
MStra.3
Associate III
December 2, 2020
Question

IOC file for LwIP_HTTP_Server_Netconn_RTOS Example project

  • December 2, 2020
  • 2 replies
  • 966 views

Is there an IOC file available for the LwIP_HTTP_Server_Netconn_RTOS Example project? I am working with the Nucleo-144 with the STM32F439ZI. Although the example project is for the 429, it works on this board. I want to be able to use CubeMX to add more middleware to the project.

Mike.

2 replies

Houssem CHAABANI
Visitor II
December 2, 2020

Dear @MStra.3​ ,

You can migrate the example from one STM32 to another by following this tutorial.

Hope that this solve your issue.

Best regards,

Houssem

MStra.3
MStra.3Author
Associate III
December 2, 2020

That is not what I asked for. I want an IOC file for the LwIP_HTTP_Server_Netconn_RTOS Example project so I can reconfigure the project using CubeMX.

Mike.

Associate
January 3, 2025

I would also like this IOC file