issue in one pulse mode in stm32f030c8t6.
Currently i am working with one pulse mode in stm32f030c8t6. TIM15, slave mode = Trigger mode,Trigger source=TI2FP2, and channel = PWM channel CH1 ,Input and output frequency 50Hz. My problem is whenever i connect the trigger input pulse,(From external optocoupler circuit) the input pulse disappears (observing with the help of CRO).And no signal at the output also.If i generate a 50Hz square pulse from the same controller and giving it to the trigger input, then the input signal level will reduce to half voltage(but it is giving the output properly). The code is given below. This code is working fine with stm32f103c836(there is no dip in the input signal level also).What is the actual problem?. help me to solve this problem.
code
--------
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_TIM15_Init();
HAL_TIM_OnePulse_Start(&htim15,TIM_CHANNEL_1);
TIM15->CCR1 =20000;//maximum value 47999//prescalar 9
while (1)
{
HAL_Delay(100);
}