LTDC Window Horizontal Stop and Vertical Stop: 800 or 799?
Hi,
when configuring the LTDC for a 800 x 800 display, the Window Horizontal Start is by default set to 0 which suggests it is a 0-indexed range. So do you set the Window Horizontal Stop and Window Vertical Stop to 800 or to 799?
As a separate question, if you use TouchGFX, are those values changed according to what you put on various pages and/or by some settings there?
Thank you :)
Rick