Skip to main content
Associate II
September 4, 2023
Solved

Make can not build project from STM32CubeMX with CMSIS_V2

  • September 4, 2023
  • 2 replies
  • 1132 views

I encountered a problem with building project from STM32CubeMX v6.9.1 with generated Makefile and CMSIS_V2 enabled. Starting build by 'make' returns an error 1 for /main.o "Can not find specified file". On the other hand, when using CMSIS_V1 everything is building without errors.
Is it something with CubeMX or CMSIS_V2 need some extra configuration, when using makefile from Cube? I am using GNU Make 3.81 for Windows and tried build it with two version of GNU Arm Compiler: v10.3-2021.10 and 9 20-q1-update.

    This topic has been closed for replies.
    Best answer by Michał M

    Wrong forum. Topic to close. Link to same question: https://community.st.com/t5/stm32cubemx-mcus/make-can-not-build-project-from-stm32cubemx-with-cmsis-v2/td-p/587662

    2 replies

    Michał MAuthorBest answer
    Associate II
    September 5, 2023
    Michał MAuthor
    Associate II
    September 11, 2023

    Is there any option, that I could use CMSIS_V2 with STM32CubeMX, or I need to change files in an other way?