Skip to main content
Florian Moser
Senior
September 22, 2022
Solved

Missing alternate function on SPI-Pins in CubeMX-generated-code.

  • September 22, 2022
  • 5 replies
  • 3227 views

uC: STM32H725AEIx

FW-Package: STM32Cube FW_H7 V1.10.0

CubeMX-Version: 6.6.1

IOC-File: Attached (SPI_bug.ioc)

I tried to generate code with CubeMX for my project. I set up SPI2 as Full-Duplex Master without hardware NSS with the follwing pin config:

  • SCK: PB13
  • MISO: PC2
  • MOSI: PC3

The code generated in `void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)` looks like the following for MOSI and MISO:

GPIO_InitStruct.Pin = SPI_MISO_Pin|SPI_MOSI_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

Although it should look like that:

GPIO_InitStruct.Pin = SPI_MISO_Pin|SPI_MOSI_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

=> The configuration for `Alternate` is missing!

With the generated code, the MOSI and MISO lines do not work at all, while the SCK is doing its thing. After the fix they work like a charm.

This topic has been closed for replies.
Best answer by Ghofrane GSOURI

Hello @Florian Moser​ 

I am glad to inform you that the Internal ticket number: 135607 is fixed and integrated in the latest CubeMX version 6.8.0 .

This is the LINK for downloading it .

Thanks again for your contributions .

Ghofrane.

5 replies

Ghofrane GSOURI
Technical Moderator
September 26, 2022

Hi @Florian Moser​ 

uC: STM32H725AEIx

FW-Package: STM32Cube FW_H7 V1.10.0

CubeMX-Version: 6.6.1

I created a project where i activated the SPI2 only (same configuration as you ) to make sure of the existence of the issue that you mentioned before ; i checked the function "HAL_SPI_MspInit" and i found The configuration for `Alternate`

0693W00000SwGQrQAN.png 

Kind regards

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Florian Moser
Senior
September 27, 2022

Thanks for your response!

It generated it for PD3 and PC1, but not for PC2 in your case.

Please try using the same GPIO as me and you will more likely run into that bug:

  • SCK: PB13
  • MISO: PC2
  • MOSI: PC3

Ghofrane GSOURI
Technical Moderator
September 27, 2022

Hi @Florian Moser​ 

I reproduced the configuration using the same  GPIO as you said

  • SCK: PB13
  • MISO: PC2
  • MOSI: PC3

0693W00000SwKRtQAN.pngI found this :

0693W00000SwKUEQA3.pngPlease have a look .

Kind regards

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Florian Moser
Senior
September 27, 2022

Thank you for reproducing!

That's exactly the bug I am describing.

For PC2 and PC3 following line is missing in the CubeMX-generated code:

GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;

(Should be between lines 116 and 117 in your screenshot code)

Without that line, the MOSI pin isn't working, it just stays low.

Hope this bug get's fixed soon!

Ghofrane GSOURI
Technical Moderator
September 28, 2022

Hi @Florian Moser​ 

Thank you for your contributions and for your detailed explanations,

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number: 135607(This is an internal tracking number and is not accessible or usable by customers).

I will keep you posted with updates.

Regards,

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Florian Moser
Senior
September 29, 2022

Thank you very much!

Ghofrane GSOURI
Ghofrane GSOURIBest answer
Technical Moderator
March 7, 2023

Hello @Florian Moser​ 

I am glad to inform you that the Internal ticket number: 135607 is fixed and integrated in the latest CubeMX version 6.8.0 .

This is the LINK for downloading it .

Thanks again for your contributions .

Ghofrane.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Florian Moser
Senior
March 8, 2023

Nice, thank you!