Missing enum values for STOP2_MODE in system_debug_signal_t cause compilation error
I am configuring to support Stop mode 2 in the stm32_wpan configuration section in the STM32CubeMX.
The following lines are generated in stm32_lpm_if.c
SYSTEM_DEBUG_SIGNAL_SET(LOW_POWER_STOP2_MODE_ENTER);
SYSTEM_DEBUG_SIGNAL_SET(LOW_POWER_STOP2_MODE_ACTIVE);
SYSTEM_DEBUG_SIGNAL_SET(LOW_POWER_STOP2_MODE_EXIT);However, the definitions of LOW_POWER_STOP2_MODE_ENTER, LOW_POWER_STOP2_MODE_ACTIVE and LOW_POWER_STOP2_MODE_EXIT don't get generated, which are causing undefined compilation errors.
I checked the expected types for these definitions, and see that these should be defined as part of the system_debug_signal_t enum inside debug_signals.h. I have tried looking for additional configurations that might generate the missing definitions but I haven't had any success so far.
What should I look into or how can I generate these missing definitions? I could try to manually add these definitions to system_debug_signal_t. but then any time I re-generate with new configurations it will get ovewritten.
I am using STM32CubeMX version 6.14.0
Toolchain: EWARM V9.20
MCU Reference:STM32WBA63CIUx.
Firmware package name and version: STM32Cube FW_WBA V1.6RC2
The project uses the STM32_WPAN and X-CUBE-FREERTOS software packs, currently trying to set the following configurations in STM32_WPAN:
CFG_LPM_LEVEL = 2
CFG_LPM_STDBY_SUPPORTED = 2 (for Stop mode 2)