Skip to main content
Associate II
July 31, 2025
Question

MX_FLASH_Init does not launch option bytes loading

  • July 31, 2025
  • 3 replies
  • 437 views
MCU: STM32H563VITx

 

Stm32CubeMX version: 6.14.0

 

HAL Driver version: 1.5.0

 

When I enable EDATA option bytes in CubeMX, it generates the following code: 
void MX_FLASH_Init(void)
{

 /* USER CODE BEGIN FLASH_Init 0 */

 /* USER CODE END FLASH_Init 0 */

 FLASH_OBProgramInitTypeDef pOBInit = {0};

 /* USER CODE BEGIN FLASH_Init 1 */

 /* USER CODE END FLASH_Init 1 */
 if (HAL_FLASH_Unlock() != HAL_OK)
 {
 Error_Handler();
 }

 /* Option Bytes settings */

 if (HAL_FLASH_OB_Unlock() != HAL_OK)
 {
 Error_Handler();
 }
 pOBInit.OptionType = OPTIONBYTE_EDATA;
 pOBInit.Banks = FLASH_BANK_2;
 pOBInit.EDATASize = 2;
 if (HAL_FLASHEx_OBProgram(&pOBInit) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_FLASH_OB_Lock() != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_FLASH_Lock() != HAL_OK)
 {
 Error_Handler();
 }

 /* Launch Option Bytes Loading */
 /*HAL_FLASH_OB_Launch(); */

 /* USER CODE BEGIN FLASH_Init 2 */

 /* USER CODE END FLASH_Init 2 */

}​

 

The function does not launch option bytes loading. The 41st line suggests that just uncommenting it should enable it but this is misleading. Running `HAL_FLASH_OB_Launch` after `HAL_FLASH_Lock` will fail as the `HAL_FLASH_OB_Launch` function does not unlock flash option bytes. The function should be placed before `
HAL_FLASH_OB_Lock` or the flash option bytes should be unlocked again. 

3 replies

KDJEM.1
Technical Moderator
August 27, 2025

Hello @continuum;

 

Could you please try with sequence and let me know if the issue is solved or not?

 if (HAL_FLASHEx_OBProgram(&FLASH_OBInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Start option byte load operation after successful programming operation */
 HAL_FLASH_OB_Launch();

 /* Lock the Flash to disable the flash control register access (recommended
 to protect the FLASH memory against possible unwanted operation)
 */
 HAL_FLASH_Lock();

 /* Lock the Flash control option to restrict register access */
 HAL_FLASH_OB_Lock();

 

Also, I recommend you to look at STM32CubeH5/Projects/NUCLEO-H563ZI/Examples/FLASH/FLASH_EDATA_EraseProgram at main · STMicroelectronics/STM32CubeH5 · GitHub example may help you to check your code.

 

I hope this help you.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KDJEM.1
Technical Moderator
September 12, 2025

Hello @continuum ;

 

Any update about the issue?

If your issue is solved,  please click on Accept as Solution on the reply which solved your issue.

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
continuumAuthor
Associate II
September 29, 2025

Hi @KDJEM.1 

Your solution probably works. I had it already figured out. My problem is how CubeMX generates the code. The commented out line with 

HAL_FLASH_OB_Launch

suggests that uncommenting this should apply option bytes which is not the case. Also, there is no user code block before HAL_FLASH_Lock where the user can place this line. 

Sramo.1
Explorer
December 17, 2025

Thank you for your help in resolving the issue. After working with EEPROM emulation, I couldn’t disable EDATA. Three days were spent before I saw your message

KDJEM.1
Technical Moderator
September 29, 2025

Hello @continuum ;

 

I reported the STM32CubeMX issue internally for checking and fixing.

Internal ticket number is reported : 218539 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you for reporting this issue and for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.