Skip to main content
Visitor II
October 27, 2023
Question

Non-secure interrupts are not working with trustzone enabled

  • October 27, 2023
  • 1 reply
  • 1004 views

CubeMX generates a file called "partition_stm32h563xx.h", this file contains the settings of which interrupts are available in the non-secure area, when trustzone is enabled.

For stm32h563 the generated list of interrupts is wrong.
There are many interrupts, which doesn't exist, while other interrupts are missing and some are in the list, but at a wrong place.

The result is many interrupts are not working in non-secure.
It can be manually changed in the "partition_stm32h563xx.h", but it has to be done every time code is generated

This topic has been closed for replies.

1 reply

Ghofrane GSOURI
Technical Moderator
November 6, 2023

 

Hello @Mogens 

First let me thank you for posting.

Actually this is a known issue and it's the subject of internal tickets.

Internal tickets number:   160379 and 162566  (This is an internal tracking number and is not accessible or usable by customers).

I'll keep you posted with the updates.

Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.