OPAMP on STM32G431KB
Hi, Master:
Hello, I want to use the opamp amplifier function of the g431kb board to connect an external gain circuit and use standlone mode. Can I use it after downloading my MXsoftware generate code?
I set the OPAMP1_P (PA7) input to 2.5V (DC power supply),
OPAMP1_M (PA3) input to 1Vpp sine wave,
plus 15K ohm R1, 33K ohm R2,
OPAMP1_P (PA7) output should be 5.8V~10.2V , is this correct?
Because the output waveform cannot be changed according to the DC power supply, the gain is always 5.
Have I not enabled the OPA function?
Thank you very much!