Skip to main content
Associate II
July 25, 2024
Question

Ram or flash size of network is bigger than available on STM32H747-DISCO

  • July 25, 2024
  • 0 replies
  • 766 views

Hello, I wanted to create a project using X-CUBE-AI and the quantized tiny yolo from model zoo (which is dedicated for deployment on STM32H747-DISCO)  : https://github.com/STMicroelectronics/stm32ai-modelzoo/tree/main/object_detection/pretrained_models/tiny_yolo_v2/ST_pretrainedmodel_public_dataset/coco_2017_person/tiny_yolo_v2_224

Though, when I analyze the project through CubeMX, the flash that will be used is too high, despite the model being already quantized.

TECO_0-1721919369016.png

Is there a proper way to reduce the flash?


I attached the .ioc file of my project.