Skip to main content
Visitor II
June 9, 2025
Question

software problem after and before update CubeMX and IDE

  • June 9, 2025
  • 2 replies
  • 362 views
software problem after and before update CubeMX and IDE

hi there

could you help me with this;

after updating CUBMX to latest one 6.14.1, does not open the project automatically , even when i open it from IDE with existing project from CUB MX option , still comes up with this error ;

 

This file has been generated with STM32CubeMX version '6.14.1'.Your current STM32CubeMX version is '6.4.0'.
Please check for update: Help > Check for Updates

 

THE FUNNY THING IS THE LATEST UPDATE FOR CUB MX IS 6.14.1 SO WHY DETECTS THE VERSION WRONG, WHICH IS NOT EXIST ( 6.4)!?

 

SO I CAN NO LUNCH PROJECT FROM CUB MX TO IDE either. 

 

could you help me with this?

 

regards

Ali10

2 replies

TDK
Super User
June 9, 2025

STM32CubeIDE has a bundled STM32CubeMX version. When you open an IOC from within STM32CubeIDE, it uses this bundled version. The only way to update the bundled STM32CubeMX it is to update STM32CubeIDE itself. You can either do that or you can leave it as-is and use the standalone STM32CubeMX to open it. Either way works.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Peter BENSCH
Technical Moderator
June 9, 2025

@Ali10 Well... from STM32CubeIDE 2.0 everything will be better and hopefully clearer.