SPI2 Frequency of the STM32F469BIT7
EMB1428QSQ/NOPB is used which has the frequency of the 1.1MHz fclk and the SPI2 of STM32F469BIT7 is going as a clock to it. I need the minimum value of the SPI2 master that can be fed to the EMB1428QSQ/NOPB. Also, where can I find the minimum frequency of the communication interfaces , I have used the USART and SPI2.