Starting with X-Nucleo-67W61M1 in CubeMX
I am setting up a project using CubeMX to evaluate the 67W61M1 device, using a Nucleo-F411RE. As far as I can tell the X-NUCLEO-67W61M1 needs SPI1 of the Nucleo for communication. Unfortunately, the Nucleo has SWO (PB3) where SPI1_SCK and while I see a solder bridge that can remove SWO from the STLink-OB, I do not see a way of disabling the SWO connection to PB3.
I tried resetting the state of PB3 in Cube MX and then I can enable SPI, however the "SYS" module then issues a warning about a conflict with SPI1 full duplex master.
Is this the correct way to configure SPI1 and Serial Debug?
Sid