STM32CubeIDE 1.15 Bug (switching from SysTick to TIM16)
I'm using the Nucleo-C031C6 board, and I chose this (NUCLEO-C031C6) from the board selector when starting the IDE. (STM32CubeIDE v1.15).
I tried switching Timebase Source (in SYS menu) from SysTick to TIM16, then when I compiled, I got this error:
../Core/Inc/stm32c0xx_hal_conf.h:237:11: fatal error: stm32c0xx_hal_tim.h: No such file or directory
It is just a bare project with no user code added.
I had to switch from SysTick to TIM16 because I was trying out ThreadX.