STM32CubeIDE hangs while attempting to open .ioc file
I have intermittent problems in STM32CubeIDE 1.8.0 opening a .ioc file. When I double click on the file in the Project Explorer, I get a progress bar titled "Loading IOC". When things are working well, as soon as that bar fills up, it is replaced with a progress bar titled "Completing IOC Load"; and when that fills up, the configuration screen is dsplayed.
Sometimes the IDE gets into a state where the first progress bar will fill up, but the second one never appears. Instead, the window hangs--I get a spinning cursor, and the Windows message "not responding". This lasts forever. If I force quit the IDE and retry, many times, eventually it starts working again.
How can I keep this from happening, and if it does happen, how can I reliably and quickly recover?