Solved
STM32CubeIDE & MX integrated
Hi,
I have some problem with STM32CubeIDE, since when I start a new project everything works well as long as I delete the file:
"home/STMCubeIDE/workspace_1-13.1/.metadata/.plugins/.org.eclipse.e4.workbench/workbench.xmi".
However, when I exit the project, closing STM32CubeIDE, and I reopen it, recalling integrated MX, either a blank page or the MCU only is shown. I'm not allowed to do anything.
STM32CubeMX standalone works correctly, without problems.
I tried to find some solution online, nothing works but deleting the file indicated above and restart the project
Here's my system informations:
Computer HP HP 250 G5 Notebook PC
SSD 500 GiB
Memory 8.0 GiB
Processor Intel® Celeron(R) CPU N3060 @ 1.60GHz × 2
Graphics card Mesa Intel® HD Graphics 400 (BSW)
O.S. Ubuntu 22.04.1 LTS 6.2.0-31-generic #31~22.04.1-Ubuntu
GNOME version 42.9
Graphics system Wayland
Java version:
openjdk version "17.0.8.1" 2023-08-24
OpenJDK Runtime Environment (build 17.0.8.1+1-Ubuntu-0ubuntu122.04)
OpenJDK 64-Bit Server VM (build 17.0.8.1+1-Ubuntu-0ubuntu122.04, mixed mode, sharing)
STM32CubeMX version 6.9.1
STM32CubeIDE version 1.13.1
STM32CubeProgrammer API v2.14.0 | Linux-64Bits
STM32 Trusted Package Creator v2.14.0 STMicroelectronics
Thanks for any suggestion.