Question
STM32CubeMX 6.11.1 released
STM32CubeMX 6.11.1 was released on st.com as well as an in-tool update patch.
Main issues fixed in this patch:
- Ticket 176645 : STM32CubeMX V6.11.0 has lost the "JTAG (5 pins)" debug mode for all the STM32H7 series but the STM32H7Rx/7Sx microcontrollers.
- Ticket 176638 : STM32CubeMX V6.11.0 has lost 3 modes for all the STM32H7 series but the STM32H7Rx/7Sx microcontrollers on ADC3
- Ticket 176658 : STM32CubeMX V6.11.0 is not generating the call to "HAL_PWREx_EnableVddA()" function for STM32U5 series.
- Ticket 177071 : Compilation error related to MX_FLASH_Init() function for STM32H5 series.
- Ticket 176763 : An issue affects ADC oversampling when writing OVSR bits for all the STM32H7 series but the STM32H7Rx/7Sx microcontrollers.
- Ticket 177285 : An error occurs when switching the timebase source from SysTick to a timer for the STM32C0 series.
Check the errata under this link for more details.
Where do I obtain STM32CubeMX 6.11.1 ?
- STM32CubeMX 6.11.1: STM32CubeMX - STM32Cube initialization code generator - STMicroelectronics
- Or in the Home view click on "Check for Updates"