Skip to main content
Associate II
May 1, 2025
Solved

STM32CubeMX 6.14.1 create project fail on STM32H7S7L8-DK with STM32Cube FW_H7RS V1.2.0

  • May 1, 2025
  • 2 replies
  • 472 views

If I select STM32CubeIDE as the toolchain, I encounter the following error during compilation. However, if I switch the toolchain to EWARM, the project compiles without any errors.

I’ve attached the .ioc file and build log for reference. Could you please help analyze what might be causing the issue?

Thank you in advance for your assistance!

Tom17_0-1746064083232.png

 

Best answer by Mahmoud Ben Romdhane

Hello @Tom17 ,

 

I suggest that you increase the flash size in STM32H7S7L8HXH_default.ld file.

 

MahmoudBenRomdhane_0-1746179806345.png

Thanks.

Mahmoud

2 replies

Technical Moderator
May 2, 2025

Hello @Tom17 ,

First let me thank you for posting and welcome to the ST Community.

Your request is under investigation, and I will get back to you ASAP.

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Technical Moderator
May 2, 2025

Hello @Tom17 ,

 

I suggest that you increase the flash size in STM32H7S7L8HXH_default.ld file.

 

MahmoudBenRomdhane_0-1746179806345.png

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.