Skip to main content
Heinz_Baumer
Associate II
November 4, 2025
Question

STM32CubeMX(6.15.0) bug for NUCLEO-H563

  • November 4, 2025
  • 2 replies
  • 147 views

Hello.

In CubeMX, there is a Bug with a wrong Clock of USART2 and a wrong BRR-Value

I've used CubeMX to configure the Clock, based on the Nucleon-H563.
For the USART2, i want to use the stable crystal oszillator (25MHz) from the Board (not the HSI-Clock)

So i configure a 125MHz-Clock on PLL2Q and set this as clock for USART2.
The Baudrate should be: 9600.


After generating code, the baudrate of USART2 ist 3078,81 Baud (measured).

 

To calculate the uart baudrate divider (USART2_BRR), MX use the: STM32Cube_FW_H5_V1.5.0\Drivers\STM32H5xx_HAL_Driver\Src\stm32h5xx_hal_uart.c


In Function: UART_SetConfig(UART_HandleTypeDef *huart) Line 3329, the usartdiv is calculated with: 407
( (125000000 / 32) + ((9600)/2)) / 9600 = 407
But with this, a wrong baudrate is generated (3078,81Baud)

 


If i use 130 as divider, the Baudrate is near correct, because the USART-Clock seems to be 39,9013776MHz instead of 125MHz .

What is the reason for the wrong clock of PLL2Q or the BRR?

Heinz_Baumer_0-1762249055656.png

Heinz_Baumer_1-1762249082004.png

 




2 replies

Technical Moderator
November 4, 2025

Hello @Heinz_Baumer ,

 

Let me thank you for posting.

Your request is under investigation, and I will get back to you as soon as possible.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Heinz_Baumer
Associate II
November 5, 2025

Hello.


I found the problem.
The PH0-OSC_IN was driven from STLINK with 8MHz, on a new Board without activating the 25MHz oszillator.

Sorry for my mistake, but I have several Nucleon boards in testing and the others had already been re-soldered, only this board hadn't.


Now it work's correct.