STM32CubeMX 6.15.0 - Bug with STM32G0B1VE not having USB-C?
I pulled down the latest CubeMX (v6.15.0) to do a parametric search for a new part. Needing > 70 GPIOs and USB device function but not much else, I narrowed in on the STM32G0B1 series.
When I start CubeMX, I'm told there are 4801 items in the parts list, When I filter on "STM32G0B1", that drops to 103 items. However... if I then filter on either "USB FS" or "USB Type-C", that number drops to 97 parts. I exported a before and after and diffed the lists, and found that the 7 parts that fell out of the list were all STM32G0B1VE parts. The 'VB (128K flash) and 'VC (256K flash) parts were in both lists, only the 'VE (512K flash) parts appeared to lack the "USB FS" and "USB Type-C" attributes.
This is a mistake, correct? The 'VE parts have all the same peripheral features as the 'VB and 'VC parts, yes?
Dana M.