Skip to main content
Associate II
July 23, 2025
Question

STM32CubeMX 6.15.0 issue

  • July 23, 2025
  • 1 reply
  • 384 views

I just updated CubeMX to 6.15.0 and I can't start a new project anymore.

The spinning wheel keeps sinning forever after going File/New Project or clicking on any on the shortcuts on the right side of the screen under "I need to:" section.

I tried to refresh data, use auto-refresh under connection and updates, etc. Nothing works.

I'm on Windows 11 Home, Version 24H2.

Older projects still work after conversion, I can still open older .ioc projects, but the dialog is asking me to migrate the project and I don't want to do that in case I need to downgrade the CubeMX application.

Is there a way to downgrade to a pervious version?

Thank you!

1 reply

vardAuthor
Associate II
July 24, 2025

I got it to work after uninstalling and re-installing everything.