STM32CubeMX 6.9.1 and STM32CubeIDE 1.13.1 released.
STM32CubeIDE 1.13.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.9.1 that is available for download.
Main issues fixed in this patch:
This patch release fixes the issues related to the following cases:
STM32CubeMX
- Ticket 157216: X-Cube-FreeRTOS: compilation Error with IAR.
- Ticket 157222: CubeMX v6.9 deletes Folder added by user when regenerating the code using MDK-ARM.
Where do I obtain CubeIDE 1.13.1, CLT 1.13.0 and CubeMX 6.9.1?
- For IDE 1.13.1: STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics
- For CLT 1.13.0: STM32CubeCLT - STM32CubeCLT is a toolset for third-party integrated development environment (IDE) providers, allowing the use of STMicroelectronics proprietary tools within their own IDE frameworks. - STMicroelectronics
- Or update your current installation of STM32CubeIDE using: Help > Check for updates.
- Updating STM32CubeIDE, the post-update restart fails. STM32CubeIDE must be restarted manually.
Related threads:
CubeMX 6.9.0 Pulls all my custom files from my Kei... - STMicroelectronics Community